Read / Write |
|
Description |
Sets or queries the connector type for the specified port. |
VB Syntax |
obj.ConnectorType (port) = value |
Variable |
(Type) - Description |
obj |
Any of the following: GuidedCalibration (object) SMCType (object) VMCType (object) |
port |
(Long) Port number of the connector type. For Guided Cals and SMC, select port number. For VMC calibrations:
|
value |
(String) - Connector type. Case-sensitive. Use ValidConnectorType Property to list connector types. |
Return Type |
String |
Default |
None |
Examples |
SMC.ConnectorType(1) = "APC 3.5 male" value = SMC.ConnectorType(1) |
C++ Syntax |
HRESULT get_ConnectorType(long port, BSTR *connector) HRESULT put_ConnectorType(long port, BSTR connector) |
Interface |
IGuidedCalibration SMCType VMCType |
Last Modified:
1-Dec-2011 |
Updated with VMC |
13-Aug-2007 |
Added detail to port argument |