Description |
Note: This command is replaced with CalKitType which sets the ECal module and User Characterization. Specifies the characterization data within an ECal module to be used for the SMC calibration. Learn more about ECal User Characterization. |
VB Syntax |
SMC.ECALCharacterization(mod) = value |
Variable |
(Type) - Description |
|
SMC |
SMCType (object) |
|
module |
1- ECal module |
|
value |
(Long) – Characterization data within the ECal module to be used for ECal operations. Choose from: 0 – Factory Characterization 1 – UserCharacterization1 2 – UserCharacterization2 3 – UserCharacterization3 4 – UserCharacterization4 5 – UserCharacterization5 |
Return Type |
Long |
Default |
0 - Factory Characterization |
Examples |
SMC.ECALCharacterization(1)= 2 |
C++ Syntax |
HRESULT put_ECALCharacterization( long moduleNumber, long characterization); HRESULT get_ECALCharacterization( long moduleNumber, long* characterization); |
Interface |
ISMCType |