Write/Read |
About FCA Calibrations |
Description |
Sets and returns the ECal or mechanical cal kit for the specified port number to be used during the calibration. There is also a CalKitType Property for use during an Unguided Cal. Note: Sliding loads are not fully supported from the GuidedCalibration object. The Measure button must be pressed manually on the PNA. Note: This command replaces Do1PortEcal Property and Do2PortEcal Property for SMC and VMC Calibrations. |
VB Syntax |
object.CalKitType (port) = value |
Variable |
(Type) - Description |
object |
Any of the following: GuidedCalibration (object) SMCType (object) VMCType (object) |
port |
(Long) Port number to which the cal kit will be assigned. For Guided Cals and SMC, select port number. For VMC calibrations:
|
value |
(string) - Calibration Kit type. Case-sensitive. Use GetCompatibleCalKits to return a list of valid Cal Kits. |
Return Type |
String |
Default |
Not Applicable |
Examples |
'Note: All of the following specify port 1 only ' Mechanical Cal Kit guidedCal.CalKitType(1) = "85052C" ' Standard ECal modules guidedCal.CalKitType(1) = "N4691-60004 ECal" ' Non-factory ECal characterizations are specified as follows: guidedCal.CalKitType(1) = "N4691-60004 User 1 ECal" ' When two or more ECal modules with the same model number are ' connected, also specify the serial number as follows: guidedCal.CalKitType(1) = "N4691-60004 ECal 01234" ' When Disk Memory ECal user characterizations are used, ' specify both the User char and the serial number as follows: 'guidedCal.CalKitType(1) = "N4691-60004 MyDskChar ECal 01234" ' Turn on auto orientation for the ECal (default behavior). |
value = smc.CalKitType(1) 'Read |
|
C++ Syntax |
HRESULT get_CalKitType( long port, BSTR *calkit) HRESULT put_CalKitType( long port, BSTR calkit) |
Interface |
IGuidedCalibration SMCType VMCType |
Last Modified:
6-Apr-2011 |
Edited Ecal Examples |
17-Feb-2011 |
Replaces Do1 and 2portECal |
13-Aug-2007 |
Added detail for port argument |