Read-only
About SA Application

ExportReceiverList Property


Description

Returns the currently exported receiver list.

Note: The list is set with ExportReceiverSetList can contain more receivers, this query will only return the ones that are currently measured and that are in the receiver list.

VB Syntax

list = sa.dft.ExportReceiverList

Variable

(Type) - Description

sa.dft

A SpectrumAnalyzerDFT (object)

list

(String) Variable to store the returned list.

Return Type

String

Example

list = sa.dft.ExportReceiverList 'Read

C++ Syntax

HRESULT get_ExportReceiverList(BSTR* ReceiverList);

Interface

ISpectrumAnalyzerDFT