Write/Read
About SA Application

ExportReceiverSetList Property


Description

Sets and returns the list of exported receivers.

Note: This list can contain receivers that are not currently measured in the channel. However, this is not an issue. To get the current list of receivers that export data, query ExportReceiverList.

VB Syntax

sa.dft.ExportReceiverSetList = list

Variable

(Type) - Description

sa.dft

A SpectrumAnalyzerDFT (object)

list

(String) Variable to store the returned list.

Return Type

String

Example

sa.dft.ExportReceiverSetList = "B" 'Write

list = sa.dft.ExportReceiverSetList 'Read

C++ Syntax

HRESULT get_ExportReceiverSetList(BSTR* ReceiverList);

HRESULT put_ExportReceiverSetList(BSTR ReceiverList);

Interface

ISpectrumAnalyzerDFT