Write/Read. |
About Trigger |
Description |
Configures the external triggering signal for the PNA and PNA-X.
|
VB Syntax |
trigsetup.ExternalTriggerConnectionBehavior (conn) = value |
Variable |
(Type) - Description |
|
trigsetup |
A TriggerSetup (object) |
|
conn |
(enum NATriggerConnection) Rear Panel connector to send or receive trigger signals. Choose from: Only one of the input connectors is active at a time. When a command is sent to one, the PNA automatically makes the other INACTIVE. 0 - naTriggerConnectionAUXT Trigger IN from rear-panel AUX IO connector Pin 19 (No longer supported. 1 - naTriggerConnectionBNC1 Trigger IN
2 - naTriggerConnectionBNC2 Trigger OUT. Only useful in point sweep mode.
3 - naTriggerConnectionMATH Trigger IN from rear-panel Material Handler connector Pin 18 4 - naTriggerConnectionBypassPulse3 - Internal routing of pulse 3 output to the MEAS TRIG IN on the rear panel. |
|
value |
(enum NAExternalTriggerBehavior) - 0 - naTriggerInactive - Disables the specified connector.
Choose from 1 through 4 when <conn> is set to naTriggerConnectionBNC1 1 - naTriggerInEdgeNegative - Triggers the PNA when receiving a negative going signal 2 - naTriggerInEdgePositive - Triggers the PNA when receiving a positive going signal 3 - naTriggerInLevelLow - Triggers the PNA when receiving a low level signal 4 - naTriggerInLevelHigh - Triggers the PNA when receiving a High-level signal
Choose from 5 through 8 when <conn> is set to naTriggerConnectionBNC2. In addition to sending this command, you must also use TriggerOutputEnabled Property to enable the BNC2 output. 5 - naTriggerOutPulsePositiveAfter - Sends a POSITIVE going TTL pulse at the END of each point during the sweep. 6 - naTriggerOutPulsePositiveBefore - Sends a POSITIVE going TTL pulse at the START of each point during the sweep. 7 - naTriggerOutPulseNegativeAfter - Sends a NEGATIVE going TTL pulse at the END of each point during the sweep. 8 - naTriggerOutPulseNegativeBefore - Sends a NEGATIVE going TTL pulse at the START of each point during the sweep. |
Return Type |
Enum as NAExternalTriggerBehavior |
Default |
BNC1 = naTriggerInactive BNC2 = naTriggerInactive
When Output is enabled BNC1 = naTriggerInactive BNC2 = naTriggerOutPulsePositiveAfter
|
Examples |
trigsetup.ExternalTriggerConnectionBehavior (naTriggerConnectionBNC1) = naTriggerInLevelLow 'Write |
|
trigBehav = trigsetup.ExternalTriggerConnectionBehavior (naTriggerConnectionAUXT) 'Read |
|
C++ Syntax |
HRESULT get_ExternalTriggerConnectionBehavior(tagNATriggerConnection connection,tagNAExternalTriggerBehavior *trigger); HRESULT put_ExternalTriggerConnectionBehavior(tagNATriggerConnection connection,tagNAExternalTriggerBehavior trigger); |
Interface |
ITriggerSetup |
Last Modified:
|
12-Apr-2012 |
Removed reference to old models |
|
12-Dec-2011 |
Added notes for models |
|
25-Feb-2008 |
Added 'Global' note |