Write/Read |
About SA Application |
Note: It is recommended that you do not use this command as it will conflict with future features.
Description |
Set and read the FFT grid dither state. |
VB Syntax |
sa.EnableDitherFFTGridOrigin = value |
Variable |
(Type) - Description |
|
sa |
A SpectrumAnalyzer (object) |
|
value |
(Boolean) Choose from: 0 - OFF - FFT grid dithering is disabled. 1 - ON - FFT grid dithering is enabled. |
Return Type |
Boolean |
Default |
0 |
Examples |
sa.EnableDitherFFTGridOrigin = 1 'Write |
|
value = sa.EnableDitherFFTGridOrigin 'Read |
|
C++ Syntax |
HRESULT put_EnableDitherFFTGridOrigin(VARIANT_BOOL bEnable); HRESULT get_EnableDitherFFTGridOrigin(VARIANT_BOOL* bEnable); |
Interface |
ISpectrumAnalyzer |