Write/Read
About SA Application

FIFOEnabled Property


Description

Enables/disables exporting data to the FIFO (First-IN, First-OUT) data buffer. FIFO is a circular buffer that allows very fast Read-Write access.

Note: FIFO commands are under the FIFO Object, and a new set of commands has been added here for binary data.

 VB Syntax

sa.dft.FIFOEnabled = value

Variable

(Type) - Description

sa.dft

A SpectrumAnalyzerDFT (object)

value

(Boolean) Choose from:

0 - OFF - Export data to FIFO disabled.

1 - ON - Export data to FIFO enabled.

Return Type

Boolean

Default

OFF

Examples

sa.dft.FIFOEnabled = ON 'Write

value = sa.dft.FIFOEnabled 'Read

C++ Syntax

HRESULT get_FIFOEnabled(VARIANT_BOOL* enable)
HRESULT put_FIFOEnabled(VARIANT_BOOL enable)

Interface

ISpectrumAnalyzerDFT