Read-only |
About PNA-X Pulsed Capabilities |
Description |
Returns the error string associated with the digital filters. The return string has three fields separated by commas: "stage1 status, stage2 status, stage3 status" Each of these fields can contain one or more of the following error codes:
|
VB Syntax |
value = spm4.FilterErrors |
Variable |
(Type) - Description |
value |
Variable to store the returned errors. |
spm4 |
A SignalProcessingModuleFour (object) |
Return Type |
String |
Default |
Not Applicable |
Examples |
mode = spm4.FilterErrors 'Read 'example return strings" NO ERROR, NO ERROR, NO ERROR *SUM-OF-COEFFICIENTS, NO ERROR, NO ERROR *COEFFICIENT *SUM-OF-COEFFICIENTS, NO ERROR, *PARAMETER |
C++ Syntax |
HRESULT get_FilterErrors(BSTR* dspErrors); |
Interface |
ISignalProcessingModuleFour |