Contains the properties for configuring the DSP (digital filters) in the PNA-X.

See the entire IF Path Block diagram.
DSP Version 5 Notes Programs that control these settings, or state files that are saved, will yield different results when run or recalled on PNAs with DSP 4 versions versus DSP 5 Versions. Stage 2 settings are IGNORED with DSP 5 Versions. |
Dim app as AgilentPNA835x.Application
Dim chan as Channel
Set chan = app.ActiveChannel
Dim digFilter as SignalProcessingModuleFour
Set digFilter = chan.SignalProcessingModuleFour
Methods |
Description |
|
|---|---|---|
None |
|
|
Properties |
Interface |
Description |
ISignalProcessingModuleFour |
Sets ADC capture mode: auto or manual |
|
ISignalProcessingModuleFour |
Returns errors with manual digital filter settings |
|
ISignalProcessingModuleFour |
Sets digital filter mode:auto or manual |
|
ISignalProcessingModuleFour |
Sets Stage1Coefficients |
|
ISignalProcessingModuleFour |
Sets Stage1 NCO frequency |
|
ISignalProcessingModuleFour |
Returns the maximum value of any single stage1coefficient. |
|
ISignalProcessingModuleFour |
Returns the maximum number of Stage1 coefficients. |
|
ISignalProcessingModuleFour |
Returns the maximum sum of all Stage1 coefficients. |
|
ISignalProcessingModuleFour |
Returns the minimum number of Stage1 coefficients |
|
ISignalProcessingModuleFour |
Sets Stage2 Coefficients |
|
ISignalProcessingModuleFour |
Returns the maximum value of any single stage2 coefficient. |
|
ISignalProcessingModuleFour |
Returns the maximum number of Stage2 coefficients |
|
ISignalProcessingModuleFour |
Returns the maximum sum of all Stage2 coefficients. |
|
ISignalProcessingModuleFour |
Returns the minimum number of Stage2 coefficients |
|
ISignalProcessingModuleFour2 |
Sets and returns Stage3Coefficients. |
|
ISignalProcessingModuleFour |
Sets and returns stage3 filter type |
|
ISignalProcessingModuleFour |
Returns the names of supported types of Stage3 filters. |
|
ISignalProcessingModuleFour2 |
Returns the maximum number of coefficients for Stage3. |
|
ISignalProcessingModuleFour2 |
Returns the maximum number of Stage3coefficients |
|
ISignalProcessingModuleFour2 |
Returns the minimum value of any single stage3coefficient. |
|
ISignalProcessingModuleFour2 |
Returns the minimum number of Stage3coefficients |
|
ISignalProcessingModuleFour |
Sets and returns the parameter value of the current filter type. |
|
ISignalProcessingModuleFour |
Returns maximum parameter value for the current filter type. |
|
ISignalProcessingModuleFour |
Returns minimum parameter value for the current filter type. |
|
ISignalProcessingModuleFour |
Returns the names of parameters for the current filter type. |
Interface |
Introduced with PNA Rev: |
ISignalProcessingModuleFour2 |
9.90 |
ISignalProcessingModuleFour |
7.2 |