Write/Read
About SA Application

ForceADCRecordSize Property


Description

Set and read the ADC record size.

VB Syntax

sa.ForceADCRecordSize = value

Variable

(Type) - Description

sa

A SpectrumAnalyzer (object)

value

(Long) Choose a value between 64 and 33554432

Learn about these settings.

Return Type

Long

Default

64

Examples

sa.ForceADCRecordSize = 256   'Write

value = sa.ForceADCRecordSize 'Read

See an example program.

C++ Syntax

HRESULT put_ForceADCRecordSize(long val);

HRESULT get_ForceADCRecordSize(long* val);

Interface

ISpectrumAnalyzer