Write/Read
About SA Application

ForceLOToFrequency Property


Description

Set and read the LO frequency.

VB Syntax

sa.ForceLOToFrequency= value

Variable

(Type) - Description

sa

A SpectrumAnalyzer (object)

value

(Double) Choose a value within the LO frequency range.

Learn about these settings.

Return Type

Double

Default

1 GHz

Examples

sa.ForceLOToFrequency= 1e9   Write

value = sa.ForceLOToFrequency 'Read

See an example program.

C++ Syntax

HRESULT put_ForceLOToFrequency(double val);

HRESULT get_ForceLOToFrequency(double* val);

Interface

ISpectrumAnalyzer