Write/Read
About SA Application

EnableImageRejectTraces Property


Description

Set and read the show / hide state of the image reject traces in the measurement parameters dialog.

VB Syntax

sa.EnableImageRejectTraces = value

Variable

(Type) - Description

sa

A SpectrumAnalyzer (object)

value

(Boolean) Choose from:

0 - OFF -Disable image reject traces.

1 - ON - Enable image reject traces and set mode using ImageReject.

Learn about these settings.

Return Type

Boolean

Default

0

Examples

sa.EnableImageRejectTraces = 0  'Write

value = sa.EnableImageRejectTraces 'Read

See an example program.

C++ Syntax

HRESULT put_EnableImageRejectTraces(VARIANT_BOOL bEnable);

HRESULT get_EnableImageRejectTracesVARIANT_BOOL* bEnable);

Interface

ISpectrumAnalyzer