Write/Read
About Mixer Configuration

InputPower Property


Description

Sets or returns the value of the Input Power.

If you are changing several mixer configuration settings, you can make all the changes first and then issue the Calculate and Apply commands as you would do from the user interface.

 VB Syntax

obj.InputPower = value

Variable

(Type) - Description

obj

A Mixer Interface pointer to the Measurement (object)

Or

A Converter Object

value

(double) - Input power in dBm.

Return Type

Double

Default

-15 dBm for IMixer

-20 dBm for IConverter

Examples

Print mixer.InputPower 'prints the value of the InputPower

C++ Syntax

HRESULT get_InputPower(double *pVal)

HRESULT put_InputPower(double newVal)

Interface

IMixer

IConverter