Read-Only
About LO Count

LOCount Property


Description

Returns the number of LO acquisitions determined by the Image Reject selection and the span.

VB Syntax

value = sa.LOCount

Variable

(Type) - Description

sa

A SpectrumAnalyzer (object)

value

(Long) Variable to store the returned number of LOs.

Learn about these settings.

Return Type

Long

Default

N/A

Examples

value = sa.LOCount 'Read

See an example program.

C++ Syntax

HRESULT get_LOCount(long* val);

Interface

ISpectrumAnalyzer