Write/Read |
About Mixer Configuration |
Description |
Sets or returns the LO sweep mode. If you are changing several mixer configuration settings, you can make all the changes first and then issue the Calculate and Apply commands as you would do from the user interface. Note: There is also a LORangeMode on the Converter Object. |
VB Syntax |
obj.LORangeMode (n) = value |
Variable |
(Type) - Description |
|
obj |
A Mixer Interface pointer to the Measurement (object) |
|
n |
(Long) - LO stage number. Choose from 1 or 2 |
|
value |
(Enum as MixerRangeMode) - LO sweep mode. Choose from: 0 - mixSwept 1 - mixFixed |
Return Type |
Enum |
Default |
0 - mixSwept |
Examples |
mixer.LORangeMode(1)=mixSwept |
C++ Syntax |
HRESULT get_LORangeMode(long LO, enum *pVal) HRESULT put_LORangeMode(long LO, enum newVal) |
Interface |
IMixer3 |
Last Modified:
|
4-Mar-2008 |
Added note. |