Write/Read
About Swept IMDx

LOStopPower Property


Description

Sets or returns the Stop value of  a LO Power sweep.  Also set imdx.SweepType to naIMDLOPowerSweep.

 VB Syntax

obj.LOStopPower (n) = value

Variable

(Type) - Description

obj

A Converter Object

n

(Long)  - LO stage number. Choose 1

value

(double) - LO Stop power in dBm.

Return Type

Double

Default

-10 dBm

Examples

convtr.LOStopPower(1) = -5 'Sets the LO Power sweep Stop value

Stop = convtr.LOStopPower(1) 'Reads the Stop value

C++ Syntax

HRESULT get_LOStopPower(long LOStage, double *pVal)

HRESULT put_LOStopPower(long LOStage, double newVal)

Interface

IConverter