MarkCoupMethPresetIsChan Property

Write/Read
About Limit Lines

Description

Set and return whether Coupled Markers is set to Channel or All after Preset. Learn more about Coupled Markers. Refer also to CoupledMarkers Property and MarkCoupPresetIsOn.

 VB Syntax

pref.MarkCoupMethPresetIsChan = value

Variable

(Type) - Description

pref

A Preferences (object)

value

(Boolean) - Choose from:

True - Marker Coupling Method is set to Channel after Preset.

False -  Marker Coupling Method is set to ALL after Preset.

Return Type

Boolean

Default

False

Examples

pref.MarkCoupMethPresetIsChan = True 'Write

value = pref.MarkCoupMethPresetIsChan 'Read

C++ Syntax

HRESULT get_MarkCoupMethPresetIsChan (VARIANT_BOOL* preference);

HRESULT put_MarkCoupMethPresetIsChan (VARIANT_BOOL val)

Interface

IPreferences15