Write/Read |
About Diff I/Q App |
Description |
Sets and reads the existing frequency ranges over which Match Correction is to be performed. On the Source Configuration dialog under Match Correction, this is the Match Frequency Range setting. |
VB Syntax |
DIQ.MatchFrequencyRange (port) = value |
Variable |
(Type) - Description |
|
DIQ |
A Differential I/Q (object) |
|
port |
(String) Source port name. Use SourcePortNames to read a list of valid source ports. |
|
value |
(String) Frequency ranges, including the "F<n>", where <n> is the range number. Separate each range with a comma. |
Return Type |
String |
Default |
Depends on <port> |
Examples |
oDIQ.MatchFrequencyRange("port 1") = "F1,F2,F3" |
|
Value = oDIQ.MatchFrequencyRange("port 2") 'Read |
|
C++ Syntax |
HRESULT get_MatchFrequencyRange(BSTR port, BSTR* MatchFrequencyRange); HRESULT put_MatchFrequencyRange(BSTR port, BSTR MatchFrequencyRange); |
Interface |
IDIQ |
Last modified:
|
24-Apr-2014 |
New topic |