Write/Read |
About Diff I/Q App |
Description |
Sets and reads the reference receiver to be used to perform Match Correction. On the Source Configuration dialog under Match Correction, this is the Reference Receiver setting. |
VB Syntax |
DIQ.MatchRefReceiver (port) = value |
Variable |
(Type) - Description |
|
DIQ |
A Differential I/Q (object) |
|
port |
(String) Source port name. Use SourcePortNames to read a list of valid source ports. |
|
value |
(String) Choose any of the reference receivers in the analyzer using logical receiver notation. Learn more. These would be "a_" where _ is the test port number. |
Return Type |
String |
Default |
Depends on <port> |
Examples |
oDIQ.MatchRefReceiver("port 1") = "a1" |
|
Value = oDIQ.MatchRefReceiver("port 2") 'Read |
|
C++ Syntax |
HRESULT get_MatchRefReceiver(BSTR port, BSTR* MatchRefReceiver); HRESULT put_MatchRefReceiver(BSTR port, BSTR MatchRefReceiver); |
Interface |
IDIQ |
Last modified:
|
24-Apr-2014 |
New topic |