Write/Read |
About Diff I/Q App |
Description |
Sets and reads the test port receiver to be used to perform Match Correction. On the Source Configuration dialog under Match Correction, this is the Test Receiver setting. |
VB Syntax |
DIQ.MatchTestReceiver (port) = value |
Variable |
(Type) - Description |
|
DIQ |
A Differential I/Q (object) |
|
port |
(String) Source port name. Use SourcePortNames to read a list of valid source ports. |
|
value |
(String) Choose any of the test port receivers in the analyzer using logical receiver notation. Learn more. These would be "b_" where _ is the test port number. |
Return Type |
String |
Default |
Depends on <port> |
Examples |
oDIQ.MatchTestReceiver("port 1") = "b1" |
|
Value = oDIQ.MatchTestReceiver("port 2") 'Read |
|
C++ Syntax |
HRESULT get_MatchTestReceiver(BSTR port, BSTR* MatchTestReceiver); HRESULT put_MatchTestReceiver(BSTR port, BSTR MatchTestReceiver); |
Interface |
IDIQ |
Last modified:
|
24-Apr-2014 |
New topic |