Read/Write
About Dynamic Uncertainty

MaximumUncertaintyPoints Property


Description

Sets and returns the maximum number of points for which uncertainties are to be computed for subsequent calibrations that are performed using Dynamic Uncertainty.

VB Syntax

uncertMan.MaximumUncertaintyPoints = value

Variable

(Type) - Description

uncertMan

An UncertaintyManager Object

value

(Boolean) Max number of points.

Return Type

Long Integer

Default

500

Examples

uncertMan.MaximumUncertaintyPoints = 201

See example program

C++ Syntax

HRESULT get_MaximumUncertaintyPoints([out,retval] long* pNumPoints);

HRESULT put_MaximumUncertaintyPoints([in] long numPoints);

Interface

IUncertaintyManager