Read-Write |
About Multiple Power Sensors |
Description |
Sets and returns the name of the Power Sensor (object) to be used as part of a Guided Power Calibration. |
VB Syntax |
pSensor.Name = value |
Variable |
(Type) - Description |
|
pSensor |
A GuidedCalibrationPowerSensor (object) |
|
value |
(string) - Name of the power sensor. The power sensor must be already configured as a PMAR device using this name. Learn how to remotely configure a PMAR device. |
Return Type |
String |
Default |
Not Applicable |
Examples |
Sensor.Name = "26GHzSesnsor" 'write value = pSensor.Name 'Read |
C++ Syntax |
HRESULT get_Name(BSTR *pPsensorName) HRESULT put_Name(BSTR pPsensorName) |
Interface |
IGuidedCalibrationPowerSensor |
Last Modified:
|
8-Feb-2011 |
New topic |