Write/Read |
About Noise Figure |
Description |
Set the bandwidth of the noise receiver. |
VB Syntax |
noise.NoiseBandwidth = value |
Variable |
(Type) - Description |
|
noise |
A NoiseFigure (object) |
|
value |
(double) Bandwidth value. For NoiseReceiver = naNoiseReceiver (Opt 029) choose from: 800 KHz, 2 MHz, 4 MHz, 8 MHz, or 24 MHz or the numerical equivalent, such as 8e6 and so forth. NOTE: The Receiver Characterization Method = "Power Meter" is NOT allowed when the Noise Bandwidth is 8 MHz or 24 MHz. For NoiseReceiver = naStandardReceiver (Opt 028) choose from: 720 kHz or 1.2 MHz If the value does not match one of these, it is rounded up to the next valid bandwidth value. |
Return Type |
Double |
Default |
4 MHz for naNoiseReceiver 1.2 MHz for naStandardReceiver |
Examples |
noise.NoiseBandwidth = 2E6 'Write |
|
NoiseBW = noise.NoiseBandwidth 'Read |
|
C++ Syntax |
HRESULT get_NoiseBandwidth(double *pVal); HRESULT put_NoiseBandwidth(double newVal); |
Interface |
INoiseFigure |
Last Modified:
|
21-May-2012 |
Edited for RcvrCharMethod |
|
21-Apr-2010 |
Added noise receiver options |
|
20-Sep-2007 |
MX New topic |