Write/Read |
About Diff I/Q App |
Description |
Sets and reads the receivers to be used to measure the phase of the sources. The phase measurement will be the difference between these two receivers. Select the receivers based on your application. You are responsible to make sure that your DUT configuration routes the signals of interest to the correct receivers. Otherwise, the phase will not be properly controlled. On the Source Configuration dialog under Phase, this is the Control Receiver setting. |
VB Syntax |
DIQ.PortPhaseParameter (port) = value |
Variable |
(Type) - Description |
|
DIQ |
A Differential I/Q (object) |
|
port |
(String) Source port name. Use SourcePortNames to read a list of valid source ports. |
|
value |
(String) Phase parameter using the following syntax: rCont/rRef Where:
Only logical receiver notation (a1,b1, etc) is available. Learn more. Enclose the entire parameter in quotes. |
Return Type |
String |
Default |
Depends on <port> |
Examples |
oDIQ.PortPhaseParameter("port 1") = "a1/a3" |
|
Value = oDIQ.PortPhaseParameter("port 2") 'Read |
|
C++ Syntax |
HRESULT get_PortPhaseParameter(BSTR port, BSTR* PortPhaseParameter); HRESULT put_PortPhaseParameter(BSTR port, BSTR PortPhaseParameter); |
Interface |
IDIQ |
Last modified:
|
24-Apr-2014 |
New topic |