Write/Read |
About Diff I/Q App |
Description |
Sets and reads the state of sweeping power. On the Source Configuration dialog under Power, this is the Sweep Power (On|Off) setting. |
VB Syntax |
DIQ.PowerSweepState (port) = value |
Variable |
(Type) - Description |
|
DIQ |
A Differential I/Q (object) |
|
port |
(String) Source port name. Use SourcePortNames to read a list of valid source ports. |
|
value |
(Boolean) Sweep Power state. Choose from:
|
Return Type |
Boolean |
Default |
False |
Examples |
oDIQ.PowerSweepState("port 2") = True |
|
Value = oDIQ.PowerSweepState("port 2") 'Read |
|
C++ Syntax |
HRESULT get_PowerSweepState(BSTR port, BOOL* PowerSweepState); HRESULT put_PowerSweepState(BSTR port, BOOL PowerSweepState); |
Interface |
IDIQ |
Last modified:
|
24-Apr-2014 |
New topic |