Read-only
About SA Application

RecordSize Property


Description

Read the current DFT record size. This value is based on the ForceADCRecordSize and dft.Type settings.

VB Syntax

value = sa.dft.RecordSize

Variable

(Type) - Description

sa.dft

A SpectrumAnalyzerDFT (object)

value

(Long) Variable to store the returned value.

Return Type

Long

Example

value = sa.dft.RecordSize 'Read

C++ Syntax

HRESULT get_RecordSize(long* val);

Interface

ISpectrumAnalyzerDFT