Write/Read
About SA Application

SourceRepeatCount Property


Description

Set and read the number of SA (receiver) sweeps for each Source Step. This setting is common to all sources.

VB Syntax

sa.SourceRepeatCount = value

Variable

(Type) - Description

sa

A SpectrumAnalyzer (object)

value

(Long)  Repeat count. Choose a value between 1 and 2e9.

Return Type

Long

Default

1

Examples

sa.SourceRepeatCount = 10   'Write

value = sa.SourceRepeatCount 'Read

See an example program.

C++ Syntax

HRESULT put_SourceRepeatCount(long count);

HRESULT get_SourceRepeatCount(long* count);

Interface

ISpectrumAnalyzer