Write/Read |
About Mixer/Converter Settings |
Description |
Sets and returns the ON|OFF state of a sweep segment. Off segments are not included is a segment sweep. Send Apply before sending a query (read). Learn more. |
VB Syntax |
conv.SegmentState(index) =state |
Variable |
(Type) - Description |
|
conv |
|
|
index |
(Long integer) Segment to set ON or OFF. Choose a segment between 1 and the current segment count. Use SegmentCount Property to read the current count in the Applied Mixer. |
|
state |
(Boolean) - Choose from: True - Segment ON False - Segment OFF |
Return Type |
Boolean |
Default |
ON when added. |
Examples |
mxr.SegmentState(1)=False 'Turns segment 1 OFF. |
C++ Syntax |
HRESULT get_SegmentState(long index, VARIANT_BOOL * val); HRESULT put_SegmentState(long index, VARIANT_BOOL val); |
Interface |
IConverter5 |
Last Modified:
|
26-Oct-2010 |
New command (A.09.33) |