Write/Read
About SA Application

SpanResolutionBWRatio Property


Description

Set and read the Frequency Span / RBW ratio.

VB Syntax

sa.SpanResolutionBWRatio = value

Variable

(Type) - Description

sa

A SpectrumAnalyzer (object)

value

(Double) Frequency Span / RBW ratio. Choose a value between 1 and 200e9.

Learn about these settings.

Return Type

Double

Default

106

Examples

sa.SpanResolutionBWRatio = 100   Write

value = sa.SpanResolutionBWRatio 'Read

See an example program.

C++ Syntax

HRESULT put_SpanResolutionBWRatio(double ratio);

HRESULT get_SpanResolutionBWRatio(double* ratio);

Interface

ISpectrumAnalyzer