Read/Write
About Dynamic Uncertainty

StandardDefinitionsEnabled Property


Description

Sets and returns the ON/OFF state of allowing the uncertainty associated with the standard definitions in the cal kits to contribute to the uncertainty of a calibration performed using Dynamic Uncertainty.  The uncertainty data for the Cal standards must also be present at the time the calibration is performed.

VB Syntax

uncertMan.StandardDefinitionsEnabled = value

Variable

(Type) - Description

uncertMan

An UncertaintyManager Object

value

(Boolean) Enable state. Choose from:

True - Standard definition uncertainty ON.

False - Standard definition uncertainty OFF.

Return Type

Boolean

Default

True

Examples

uncertMan.StandardDefinitionsEnabled = True

See example program

C++ Syntax

HRESULT get_StandardDefinitionsEnabled([out,retval] VARIANT_BOOL* pState);

HRESULT put_StandardDefinitionsEnabled([in] VARIANT_BOOL state);

Interface

IUncertaintyManager