Write/Read |
About PNA-Pulse Generators |
Description |
Enables / Disables subpoint triggering. When enabled and performing Point Averaging, Each rising edge of P0 triggers a subpoint (one of N acquisitions in an N point average). Must also enable the P0 generator using pulse.State(n). |
VB Syntax |
pulse.SubPointTrigger(n) = value |
Variable |
(Type) - Description |
|
pulse |
A PulseGenerator (object) |
|
n |
(Integer) Pulse generator number. Must be 0 as this is the generator that triggers the ADC. |
|
value |
(Boolean) Enable or disable SubPointTrigger
|
Return Type |
Boolean |
Default |
False |
Examples |
pulse.SubPointTrigger(0) = True 'Write |
|
bool = pulse.SubPointTrigger(0) 'Read |
|
C++ Syntax |
HRESULT get_SubPointTrigger (integer pulse, VARIANT_BOOL* on_off);. HRESULT put_SubPointTrigger (integer pulse, VARIANT_BOOL on_off); |
Interface |
IPulseGenerator2 |
Last Modified:
|
20-Jul-2009 |
MX New topic |