Write/Read |
About Sweep Delay |
Description |
Specifies the time to wait just before acquisition begins for each sweep. This delay is in addition to Dwell Time and the following two External Trigger delays if enabled.
|
VB Syntax |
chan.SweepDelay = value |
Variable |
(Type) - Description |
|
chan |
Channel (object) |
|
value |
(double) - Sweep delay in seconds. |
Return Type |
Double |
Default |
0 |
Examples |
chan.SweepDelay = 3e-3 'Write |
|
swpdelay = chan.SweepDelay 'Read |
|
C++ Syntax |
HRESULT get_SweepDelay(double *pVal) HRESULT put_SweepDelay(double newVal) |
Interface |
IChannel |
Last Modified:
|
6-Mar-2012 |
Fixed link |
|
1-Mar-2010 |
MX New topic |