Read/Write |
|
Description |
This command is replaced by PathThruMethod Property. Sets and returns the method for performing the thru portion of the calibration. |
VB Syntax |
obj.ThruCalMethod = value |
Variable |
(Type) - Description |
|
obj |
SMCType (object) or VMCType (object) |
|
value |
(String) Specifies the Thru method. Case insensitive - include spaces. Choose from: "Default" "Flush Thru" or "FLUSH" "Unknown Thru" or "UNKN" "Adapter Removal" or "ADAP" |
Return Type |
String |
Default |
Default |
Examples |
SMC.ThruCalMethod = "UNKN" |
C++ Syntax |
HRESULT put_ThruCalMethod(enum NAThruCalMethod thruMethod); HRESULT get_ThruCalMethod(enum NAThruCalMethod *thruMethod); |
Interface |
SMCType VMCType |