Write/Read
About Triggering ADC

TriggerADCLevelValue Property


Description

Set and read the ADC trigger level.

VB Syntax

sa.TriggerADCLevelValue = value

Variable

(Type) - Description

sa

A SpectrumAnalyzer (object)

value

(Long) Choose a value between 0 and 16383.

Learn about these settings.

Return Type

Long

Default

100

Examples

sa.TriggerADCLevelValue = 256   'Write

value = sa.TriggerADCLevelValue 'Read

See an example program.

C++ Syntax

HRESULT put_TriggerADCLevelValue(long val);

HRESULT get_TriggerADCLevelValue(long* val);

Interface

ISpectrumAnalyzer