Write/Read |
About Auxiliary TriggeringAbout Pulse Generators |
Description |
Specifies the polarity of the trigger IN signal.
Note: Used on PNA-X ONLY. |
VB Syntax |
object.TriggerInPolarity = value |
Variable |
(Type) - Description |
|
object |
An AuxTrigger (object) or A PulseGenerator (object) |
|
value |
(enum NATriggerPolarity) - Choose from: naTriggerPositive PNA responds to rising edge or HIGH level naTriggerNegative PNA responds to falling edge or LOW level. Set Edge or Level triggering using TriggerInType Property |
Return Type |
Enum |
Default |
AuxTriggerIn Object - naTriggerNegative PulseGenerator Object - naTriggerPositive. Also the polarity used when the PNA-X does not have the required DSP hardware |
Exaamples |
obj.TriggerInPolarity = naTriggerPositive 'Write |
|
value = obj.TriggerInPolarity 'Read the value |
|
C++ Syntax |
HRESULT get_TriggerInPolarity(enum NATriggerPolarity *val); |
Interface |
IAuxTrigger IPulseGenerator3 |