Write/Read |
About Auxiliary TriggeringAbout PulseGenerators |
Description |
Specifies the type of trigger input being supplied to the PNA.
Note: Use on PNA-X ONLY. |
VB Syntax |
obj.TriggerInType = value |
Variable |
(Type) - Description |
|
obj |
An AuxTrigger (object) or A PulseGenerator (object |
|
value |
(enum NATriggerSignalType) Choose from: naTriggerEdge PNA responds to the edge (rising or falling) of a signal naTriggerLevel PNA responds to the level (HIGH or LOW) of a signal Use TriggerInPolarity to set Positive or Negative polarity. |
Return Type |
Enum |
Default |
naTriggerLevel - Also the type used for the PulseGenerator Object when the PNA-X does not have the required DSP hardware |
Exaamples |
obj.TriggerInType = naTriggerEdge 'Write |
|
value = obj.TriggerInType 'Read the value |
|
C++ Syntax |
HRESULT get_TriggerInType(enum NATriggerSignalType *val); |
Interface |
IAuxTrigger IPulseGenerator3 |