Write/Read
About Periodic Counter

TriggerPeriodicCounterValue Property


Description

Set and read the periodic counter value. This command initiates a measurement trigger event based on the specified period.

VB Syntax

sa.TriggerPeriodicCounterValue = value

Variable

(Type) - Description

sa

A SpectrumAnalyzer (object)

value

(Long) Choose a value between 0 and 2147483647.

Learn about these settings.

Return Type

Long

Default

256

Examples

sa.TriggerPeriodicCounterValue = 256   'Write

value = sa.TriggerPeriodicCounterValue 'Read

See an example program.

C++ Syntax

HRESULT put_TriggerPeriodicCounterValue(long val);

HRESULT get_TriggerPeriodicCounterValue(long* val);

Interface

ISpectrumAnalyzer