Write/Read
About Vector Averaging

VectorAverageValue Property


Description

Set and read the vector averaging value.

VB Syntax

sa.coherence.VectorAverageValue = value

Variable

(Type) - Description

sa.coherence

A SpectrumAnalyzerCoherence (object)

value

(Double) Choose a value between 0 and 65536.

Learn about these settings.

Return Type

Double

Default

1 (no averaging)

Examples

sa.coherence.VectorAverageValue = 1   Write

value = sa.coherence.VectorAverageValue 'Read

See an example program.

C++ Syntax

HRESULT put_VectorAverageValue(double val);

HRESULT get_VectorAverageValue(double* val);

Interface

ICoherenceSA