Specifies settings for embedding and de-embedding Single-Ended (2-port) fixturing circuits.
CALCulate:FSIMulator:SENDed: DEEMbed PORT PMCircuit PORT PARameters ZCONversion PORT |
Click on a keyword to view the command details.
See Also
Note: CALC:FSIM commands affect ALL measurements on the specified channel.
CALCulate<cnum>:FSIMulator:SENDed:DEEMbed:PORT<n>:SNP:REVerse <bool>
(Read-Write) Set and read whether or not to reverse ports on a 2-port fixture or adapter to be de-embedded. Learn more. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<port> |
PNA port number to which SNP file is to be de-embedded. |
<bool> |
Choose from: ON or 1 - Reverse ports OFF or 0 - Do NOT Reverse ports |
Examples |
CALC:FSIM:SEND:DEEM:PORT1:SNP:REV
1 |
Query Syntax |
CALCulate<cnum>:FSIMulator:SENDed:DEEMbed:PORT<n>:SNP:REVerse? |
Return Type |
Boolean |
OFF |
|
CALCulate<cnum>:FSIMulator:SENDed:DEEMbed:PORT<n>[:TYPE] <char>
(Read-Write) Select whether or not to load a 2-port De-embedding circuit model for the specified port number. Circuit model USER is valid when an associated .s2p file is specified with CALC:FSIM:SEND:DEEM:PORT1:USER:FILename. Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<port> |
Port number to receive circuit model. |
<char> |
Choose from: NONE - Port does not have a circuit model. USER - Circuit model for the port will be loaded from PNA drive. |
Examples |
CALC:FSIM:SEND:DEEM:PORT1
USER |
Query Syntax |
CALCulate<cnum>:FSIMulator:SENDed:DEEMbed:PORT<n>[:TYPE]? |
Return Type |
Character |
None |
|
CALCulate<cnum>:FSIMulator:SENDed:DEEMbed:PORT<n>:USER:FILename <string>
(Read-Write) Specifies the filename of the circuit model to be used for de-embedding. Circuit model is applied when both CALC:FSIM:SEND:DEEM:PORT1 USER is selected and the filename is specified with this command. Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<port> |
Port number to receive circuit model. |
<string> |
File name and extension (.s2P) of the de-embedding circuit. Files are stored in the default folder "C:/Program Files/Keysight/Network Analyzer/Documents To recall from a different folder, specify the full path name. |
Examples |
CALC:FSIM:SEND:DEEM:PORT1:USER:FIL
'myFile.s2P' |
Query Syntax |
CALCulate<cnum>:FSIMulator:SENDed:DEEMbed:PORT<n>:USER:FILename? |
Return Type |
String |
Not Applicable |
|
CALCulate<cnum>:FSIMulator:SENDed:DEEMbed:STATe <bool>
(Read-Write) Turns de-embedding ON or OFF for all ports on the specified channel. Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<bool> |
Choose from: ON or 1 - Turns de-embedding ON OFF or 0 - Turns de-embedding OFF |
Examples |
CALC:FSIM:SEND:DEEM:STAT
1 |
Query Syntax |
CALCulate<cnum>:FSIMulator:SENDed:DEEMbed:STATe? |
Return Type |
Boolean |
OFF |
|
CALCulate<cnum>:FSIMulator:SENDed:OORDer <a,b,c,d>
(Read-Write) Sets and returns the order in which Single-ended Fixture Operations occur. Learn more about these operations. Note: The operation for ground loop embedding and ground loop de-embedding will always occur as the 3rd step. It cannot be moved. By default, this is after the 2-Port DeEmbedding operation. Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<a,b,c,d> |
Order of operations, where: 0 - Port Extension operation 1 - 2-Port DeEmbedding operation 2 - Port Matching operation 3 - Arbitrary Impedance operation |
Examples |
CALC:FSIM:SEND:OORD
1,2,3,0 |
Query Syntax |
CALCulate<cnum>:FSIMulator:SENDed:OORDer? |
Return Type |
Comma-separated values |
0,1,2,3 |
|
CALCulate<cnum>:FSIMulator:SENDed:PMCircuit:PORT<n>:PARameters:C <value>
(Read-Write) Sets and returns the value for the 'C' (Capacitance) circuit element for a port matching circuit model to simulate on port 'n'. The port matching circuit model is selected using CALCulate<cnum>:FSIMulator:SENDed:PMCircuit:PORT<n>[:TYPE]<char>. You can specify C, C1, or C2 based on the selected port matching circuit model. Setting a value not used by the selected circuit will have no affect. Learn more. There are three steps to set up a port matching circuit model simulation on a specified port:
Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. If unspecified, <cnum> is set to 1. |
<port> |
Port number to receive value. |
<value> |
Capacitance value in farads. Choose a value between -1E18 to 1E18 |
Examples |
CALC:FSIM:SEND:PMC:PORT1:PAR:C
0.00002 |
Query Syntax |
CALCulate<cnum>:FSIMulator:SENDed:PMCircuit:PORT<n>:PARameters:C? |
Return Type |
Numeric |
0 |
|
CALCulate<cnum>:FSIMulator:SENDed:PMCircuit:PORT<n>:PARameters:G <value>
(Read-Write) Sets and returns the value for the 'G' (Conductance) circuit element for a port matching circuit model to simulate on port 'n'. The port matching circuit model is selected using CALCulate<cnum>:FSIMulator:SENDed:PMCircuit:PORT<n>[:TYPE]<char>. You can specify G, G1, or G2 based on the selected port matching circuit model. Setting a value not used by the selected circuit will have no affect. Learn more. There are three steps to set up a port matching circuit model simulation on a specified port:
Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. If unspecified, <cnum> is set to 1. |
<port> |
Port number to receive value. |
<value> |
Conductance value in siemens. Choose a value between -1E18 to 1E18 |
Examples |
CALC:FSIM:SEND:PMC:PORT1:PAR:G
0.00002 |
Query Syntax |
CALCulate<cnum>:FSIMulator:SENDed:PMCircuit:PORT<n>:PARameters:G? |
Return Type |
Numeric |
0 |
|
CALCulate<cnum>:FSIMulator:SENDed:PMCircuit:PORT<n>:PARameters:L <value>
(Read-Write) Sets and returns the value for the 'L' (Inductance) circuit element for a port matching circuit model to simulate on port 'n'. The port matching circuit model is selected using CALCulate<cnum>:FSIMulator:SENDed:PMCircuit:PORT<n>[:TYPE]<char>. You can specify L, L1, or L2 based on the selected port matching circuit model. Setting a value not used by the selected circuit will have no affect. Learn more. There are three steps to set up a port matching circuit model simulation on a specified port:
Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. If unspecified, <cnum> is set to 1. |
<port> |
Port number to receive value. |
<value> |
Inductance value in henries. Choose a value between -1E18 to 1E18 |
Examples |
CALC:FSIM:SEND:PMC:PORT1:PAR:L
0.00002 |
Query Syntax |
CALCulate<cnum>:FSIMulator:SENDed:PMCircuit:PORT<n>:PARameters:L? |
Return Type |
Numeric |
0 |
|
CALCulate<cnum>:FSIMulator:SENDed:PMCircuit:PORT<n>:PARameters:R <value>
(Read-Write) Sets and returns the value for the 'R' (Resistance) circuit element for a port matching circuit model to simulate on port 'n'. The port matching circuit model is selected using CALCulate<cnum>:FSIMulator:SENDed:PMCircuit:PORT<n>[:TYPE]<char>. You can specify R, R1, or R2 based on the selected port matching circuit model. Setting a value not used by the selected circuit will have no affect. Learn more. There are three steps to set up a port matching circuit model simulation on a specified port:
Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. If unspecified, <cnum> is set to 1. |
<port> |
Port number to receive value. |
<value> |
Resistance value in ohms. Choose a value between -1E18 to 1E18 |
Examples |
CALC:FSIM:SEND:PMC:PORT1:PAR:R
0.00002 |
Query Syntax |
CALCulate<cnum>:FSIMulator:SENDed:PMCircuit:PORT<n>:PARameters:R? |
Return Type |
Numeric |
0 |
|
CALCulate<cnum>:FSIMulator:SENDed:PMCircuit:PORT<n>[:TYPE] <char>
(Read-Write) Select whether or not to load a 2 port matching circuit model for the specified port number. Circuit model USER is valid when an associated .s2p file is specified with CALC:FSIM:SEND:PMC:PORT1:USER:FIL Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. If unspecified, <cnum> is set to 1. |
<port> |
Port number to receive circuit model. |
<char> |
Circuit model. Choose from NONE No circuit model SLPC Series L - Parallel C PCSL Parallel C - Series L PLSC Parallel L - Series C SCPL Series C - Parallel L PLPC Parallel L - Parallel C USER Load S2P file |
Examples |
CALC:FSIM:SEND:PMC:PORT1:USER |
Query Syntax |
CALCulate<cnum>:FSIMulator:SENDed:PMCircuit:PORT<n>[:TYPE]? |
Return Type |
Character |
None - No circuit model |
|
CALCulate<cnum>:FSIMulator:SENDed:PMCircuit:PORT<n>:USER:FILename <string>
(Read-Write) Specifies the filename of the circuit model to be used for port matching. Circuit model is applied when both CALC:FSIM:SEND:PMC:PORT1 USER is selected and the filename is specified with this command. Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<port> |
Port number to receive circuit model. |
<string> |
File name and extension (.s2P) of the de-embedding circuit. Files are stored in the default folder "C:/Program Files/Keysight/Network Analyzer/Documents To recall from a different folder, specify the full path name. |
Examples |
CALC:FSIM:SEND:PMC:PORT1:USER:FIL
'myFile.s2P' |
Query Syntax |
CALCulate<cnum>:FSIMulator:SENDed:PMCircuit:PORT<n>:USER:FILename? |
Return Type |
String |
Not Applicable |
|
CALCulate<cnum>:FSIMulator:SENDed:PMCircuit:STATe <bool>
(Read-Write) Turns Port Matching ON or OFF for all ports on the specified channel. Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<bool> |
Choose from: ON or 1 - Turns Port Matching ON OFF or 0 - Turns Port Matching OFF |
Examples |
CALC:FSIM:SEND:PMC:STAT
1 |
Query Syntax |
CALCulate<cnum>:FSIMulator:SENDed:PMCircuit:STATe? |
Return Type |
Boolean |
OFF |
|
CALC<cnum>:FSIM:SEND:POW:PORT<n>:COMP <bool>
(Read-Write) Adjusts the source power at the specified port by the combined amount of loss through ALL enabled fixturing operations. Use this function to set the power level at the DUT input. Learn more. Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<port> |
Port number to receive power compensation. |
<bool> |
Choose from: ON or 1 - Compensate source power OFF or 0 - Do NOT compensate source power |
Examples |
CALC:FSIM:SEND:POW:PORT1:COMP
1 |
Query Syntax |
CALC<cnum>:FSIM:SEND:POW:PORT<n>:COMP? |
Return Type |
Boolean |
OFF |
|
CALCulate<cnum>:FSIMulator:SENDed:ZCONversion:PORT<n>:IMAG <value>
(Read-Write) Sets and returns the Imaginary portion of the impedance value for the specified single-ended port. Use CALC:FSIM:SEND:ZCON:PORT:REAL to set the real value. Or use CALC:FSIM:SEND:ZCON:PORT:Z0 to set both values together. Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<n> |
Port number to receive value. |
<value> |
Imaginary impedance value. Choose a value between -1E18 and 1E18 |
Examples |
CALC:FSIM:SEND:ZCON:PORT1:IMAG
75 |
Query Syntax |
CALCulate<cnum>:FSIMulator:SENDed:ZCONversion:PORT<n>:IMAG? |
Return Type |
Numeric |
0 |
|
CALCulate<cnum>:FSIMulator:SENDed:ZCONversion:PORT<n>:REAL <value>
(Read-Write) Sets and returns the Real portion of the impedance value for the specified single-ended port. Use CALC:FSIM:SEND:ZCON:PORT:IMAG to set the imaginary value. Or use CALC:FSIM:SEND:ZCON:PORT:Z0 to set both values together. Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<n> |
Port number to receive value. |
<value> |
Real Impedance value in ohms. Choose a value between 0 to 1E7 |
Examples |
CALC:FSIM:SEND:ZCON:PORT1:REAL
51 |
Query Syntax |
CALCulate<cnum>:FSIMulator:SENDed:ZCONversion:PORT<n>:REAL? |
Return Type |
Numeric |
50 |
|
CALCulate<cnum>:FSIMulator:SENDed:ZCONversion:PORT<n>:Z0[:R] <value>
(Read-Write) Sets and returns the Real portion of the impedance value for the specified single-ended port. The imaginary portion is automatically set to 0.0. To set both values separately, use CALC:FSIM:SEND:ZCON:PORT:REAL and CALC:FSIM:SEND:ZCON:PORT:IMAG. Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<n> |
Port number to receive value. |
<value> |
Port Impedance value in ohms. Choose a value between 0 to 1E7 |
Examples |
CALC:FSIM:SEND:ZCON:PORT1:Z0
51 |
Query Syntax |
CALCulate<cnum>:FSIMulator:SENDed:ZCONversion:PORT<n>:Z0[:R]? |
Return Type |
Numeric |
50 |
|
CALCulate<cnum>:FSIMulator:SENDed:ZCONversion:STATe <bool>
(Read-Write) Turns Port Impedance ON or OFF for all ports on the specified channel. Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<bool> |
Choose from: ON or 1 - Turns Port Impedance ON OFF or 0 - Turns Port Impedance OFF |
Examples |
CALC:FSIM:SEND:ZCON:STAT
1 |
Query Syntax |
CALCulate<cnum>:FSIMulator:SENDed:ZCONversion:STATe? |
Return Type |
Boolean |
OFF |
|
Last Modified:
3-Feb-2014 |
Fixed tree |
20-May-2011 |
Fixed SNP syntax |
12-Nov-2010 |
Added SNP reverse |
2-Feb-2009 |
Added OORDer |