|
SENSe:BANDwidth: |
See Also
|
(Read-Write) Sets the bandwidth of the digital IF filter to be used in the measurement. (Use either Sense:Bandwidth or Sense:Bwidth) |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<num> |
IF Bandwidth in Hz. The list of valid IF Bandwidths is different depending on the PNA model. (Click to see the lists.) If an invalid number is specified, the analyzer will round up to the closest valid number. This parameter supports MIN and MAX as arguments. Learn more. |
|
Examples |
SENS:BWID 1KHZ |
|
Query Syntax |
SENSe<cnum>:BANDwidth | BWIDth[:RESolution]? |
|
Return Type |
Numeric |
|
Varies with PNA model. |
|
SENSe<cnum>:BANDwidth | BWIDth:TRACk <bool>
|
(Read-Write) Sets and returns the state of the Reduce IF BW at Low Frequencies feature. (Use either Sense:Bandwidth:Track or Sense:Bwidth:Track). |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<bool> |
Choose from: ON or 1 - Reduce IF BW at Low Frequencies is set ON OFF or 0 - Reduce IF BW at Low Frequencies is set OFF |
|
Examples |
SENS:BWID:TRAC OFF |
|
Query Syntax |
SENSe<cnum>:BANDwidth | BWIDth:TRACk? |
|
Return Type |
Boolean |
|
ON |
|
Last Modified:
|
7-May-2012 |
Removed Preset |
|
15-Jan-2008 |
MIN and MAX added |