This VB Script example creates a calibrated SMC fixed output measurement using an external, controlled LO. Then a single sweep is taken and data is retrieved. The external LO is NOT required when using the internal second PNA source for the LO.
Requirements:
The external LO should be configured to match the SENS:MIX:LO:NAME command below.
Fixed output measurements require that an external LO source be swept and synchronized with the PNA source. FCA performs this synchronization using the external source configuration settings. See Configure an External Source using SCPI.
The fastest, and recommended, method of controlling the LO source is Hardware List (BNC) triggering mode. However, in this mode, FCA channels will not respond to manual triggers. Therefore, the example uses the following mechanism to trigger a sweep:
Write "SENS:SWE:MODE HOLD" 'place channel 1 in HOLD mode
Write "INIT:CONT ON" 'place PNA in internal trigger mode
Write "SENS:SWE:MODE SINGle
Write "*OPC?" 'wait until the sweep is complete
Read
The SCPI commands in this example are sent over a COM interface using the SCPIStringParser object. You can run a VBScript (*.vbs) program from the PNA using Macros. To run this program, copy the following code into a text editor and save it as a *.vbs file.
|
option explicit ' Setup infrastructure to use the SCPI over COM dim app set app = createobject("Agilentpna835x.application") dim p set p = app.scpistringparser dim returnStr sub Write (command) if len(returnStr) <> 0 then err.Raise 55,"Write","Query Unterminated" end if returnStr = p.parse(command) end sub sub WriteIgnoreError(command) returnStr = p.Execute(command) p.Parse("SYST:ERR?") ' clear error queue end sub function Read if len(returnStr) = 0 then err.Raise 55,"Read","Bad read" end if Read = returnStr returnStr = "" end function Write "SYST:PRES" ' When programming in remote mode, hold mode is recommended Write "SENS:SWE:MODE HOLD" ' Delete the standard measurement Write "CALC:PAR:DEL:ALL" ' Create an SC21 measurement Write "CALC:CUST:DEF 'MySC21', 'Scalar Mixer/Converter', 'SC21'" Write "DISP:WIND:TRACE:FEED 'MySC21'" Write "CALC:PAR:SEL 'MySC21'" ' Set number of points to 11 Write "SENS:SWE:POIN 11" ' Setup the mixer parameters for a swept LO, fixed output measurement Write "SENS:MIX:INP:FREQ:START 200e6" Write "SENS:MIX:INP:FREQ:STOP 700e6" Write "SENS:MIX:LO:FREQ:MODE Swept" Write "SENS:MIX:OUTPUT:FREQ:FIX 3.4e9" Write "SENS:MIX:OUTP:FREQ:SID HIGH" Write "SENS:MIX:CALC LO_1" Write "SENS:MIX:INP:POW -17" Write "SENS:MIX:LO:POW 10" Write "SENS:MIX:APPLY ' Specify the LO name, for controlled LO. ' This name is setup in the External Source Config Dialog Write "SENS:MIX:LO:NAME '8360'" Write "SENS:MIX:APPLY ' Create an S11 in the same channel Write "CALC:CUST:DEF 'MyS11', 'Scalar Mixer/Converter', 'S11'" Write "DISP:WIND:TRACE2:FEED 'MyS11'" Write "CALC:PAR:SEL 'MyS11'" ' Create an IPwr in the same channel Write "CALC:CUST:DEF 'MyIPwr', 'Scalar Mixer/Converter', 'IPwr'" Write "DISP:WIND:TRACE3:FEED 'MyIPwr'" Write "CALC:PAR:SEL 'MyIPwr'" ' Create an OPwr in the same channel Write "CALC:CUST:DEF 'MyOPwr', 'Scalar Mixer/Converter', 'OPwr'" Write "CALC:PAR:SEL 'MyOPwr'" Write "DISP:WIND:TRACE4:FEED 'MyOPwr'" ' Perform a single sweep, synchronously. When *OPC returns, the sweep is done Write "SENS:SWE:MODE SINGle" Write "*OPC?" Read ' Retrieve the SC21 data Write "CALC:PAR:SEL 'MySC21'" Write "CALC:DATA? SDATA" dim data data = Read() wscript.echo("SC21=" & data) 'Retrieve the S11 data Write "CALC:PAR:SEL 'MyS11'" Write "CALC:DATA? SDATA" data = Read() wscript.echo("S11=" & data) |
Last Modified:
|
8-Mar-2011 |
Updated with new SMC commands A.09.33. |