The following example program sets up a 1-stage mixer, then performs a full VMC calibration.
By removing the comments ( ' ) at the start of the BLUE code, it can also do the following:
Load a mixer setup file
Use an ECal Module
Perform manual ECal orientation
Load a Mixer Characterization
Example - Perform a Mixer Characterization ONLY
This VBScript (*.vbs) program can be run as a macro in the PNA. To do this, copy the following code into a text editor file such as Notepad and save it on the PNA hard drive as VMC.vbs. Learn how to setup and run the macro.
|
Dim app Dim scpi ' Create / Get the PNA application. Set app = CreateObject("AgilentPNA835x.Application") Set scpi = app.ScpiStringParser scpi.Parse "SYSTem:PRESet"
'Create a Vector Mixer Measurement 'First, delete all measurements on the channel scpi.Parse "CALC:PAR:DEL:ALL" 'Create a forward scalar mixer measurement and configure it in channel 1. 'The first parameter is a unique identifying string to allow subsequent 'commands to be directed at this specific measurement. scpi.Parse "CALC:CUST:DEF 'My VC21', 'Vector Mixer/Converter', 'VC21'" 'Setup the new measurement as the 2nd trace in the active window scpi.Parse "DISP:WIND:TRAC2:FEED 'My VC21'" 'Make the new trace the active measurement scpi.Parse "CALC:PAR:SEL 'My VC21'" 'The parameters of the mixer measurement can now be configured. 'This can be done by either using the SENS:MIX commands 'for each of the parameters or by loading a mixer setup file. 'Uncomment the following line to load a mixer setup file. The path 'name for the mixer file may be loaded from other mapped drives. 'scpi.Parse "SENS:MIXer:Load 'c:\users\public\network analyzer\documents/Mixer/MyMixer.mxr'"
' Setup Stimulus ' Points and IFBW are channel settings scpi.Parse "SENS:SWEep:POINts 21" scpi.Parse "SENS:BANDwidth 1e3" ' The rest are mixer settings scpi.Parse "SENS:MIX:LO:FREQ:MODE SWEPt" scpi.Parse "SENS:MIX:INPut:FREQ:STAR 3.6e9" scpi.Parse "SENS:MIX:INPut:FREQ:STOP 3.9e9" scpi.Parse "SENS:MIX:LO:FREQ:MODE FIXED" scpi.Parse "SENS:MIX:LO:FREQ:FIX 1e9" scpi.Parse "SENS:MIX:LO:POW 10" scpi.Parse "SENS:MIX:OUTP:FREQ:SID LOW" scpi.Parse "SENS:MIX:CALC Output" scpi.Parse "SENS:MIX:LO:NAME 'Port 3'" scpi.Parse "SENS:MIX:APPLY"
' Perform Cal
' Define the DUT connectors for at ports 1 and 2 of the PNA scpi.Parse "sens:corr:coll:guid:conn:port1 'APC 3.5 female'" scpi.Parse "sens:corr:coll:guid:conn:port2 'APC 3.5 male'" scpi.Parse "sens:corr:coll:guid:conn:port3 'Not used'" scpi.Parse "sens:corr:coll:guid:conn:port4 'Not used'"
' Specify Mechanical cal kits scpi.Parse "sens:corr:coll:guid:ckit:port1 '85033D/E'" scpi.Parse "sens:corr:coll:guid:ckit:port2 '85033D/E'"
' Specify an ECal module the same way 'scpi.Parse "sens:corr:coll:guid:ckit:port1 'N4691-60004 ECal'" 'scpi.Parse "sens:corr:coll:guid:ckit:port2 'N4691-60004 ECal'" ' Non-factory characterizations are specified as follows: 'scpi.Parse "sens:corr:coll:guid:ckit:port2 'N4691-60004 User 1 ECal'" ' When two or more ECal modules with the same model number are connected ' also specify the serial number as follows: 'scpi.Parse "sens:corr:coll:guid:ckit:port2 'N4691-60004 ECal 01234'" ' When Disk Memory ECal user characterizations are used, ' specify both the User char and the serial number as follows: 'scpi.Parse "sens:corr:coll:guid:ckit:port2 'N4691-60004 MyDskChar ECal 01234'" ' ' By default, VMC requires the measurement of a Calibration Mixer. ' To determine the conversion loss of the calmixer, the cal wizard ' will add a step to perform a 1 port cal at the output of the mixer. ' The following commands opt to perform the mixer ' characterization using a cal kit. scpi.Parse "SENS:CORR:COLL:GUID:VMC:MIX:CHAR:CAL:OPT CKIT" ' Define the DUT connectors for the output of the characterization mixer ' Use (logical) Port 3. If it is already used by the DUT, ' then specify port 4. scpi.Parse "sens:corr:coll:guid:conn:port3 'APC 3.5 male'" ' Specify the mechanical cal kit for port 3 scpi.Parse "sens:corr:coll:guid:ckit:port3 '85033D/E'" ' To avoid performing the 1-port cal, provide the cal wizard with a ' mixer characterization file. Uncomment the following line to ' specify the characterization file. This S2P file will be read. 'scpi.Parse "SENS:CORR:COLL:GUID:VMC:MIX:CHAR:CAL:OPT FILE,'c:\users\public\network analyzer\documents/MyMixer.s2p'"
' ECal orientation ' By default, auto orientation of the ecal module is performed ' Uncomment the following lines to manually orient the ecal 'scpi.Parse "SENS:CORR:PREF:ECAL:ORI OFF" ' for 2-port portion, ecal port A connected to PNA port 1 'scpi.Parse "SENS:CORR:PREF:ECAL:PMAP ECAL2 ="A1,B2" 'for mixer char, ecal port A connected to cal mixer output 'scpi.Parse "SENS:CORR:COLL:GUID:VMC:MIXer:ECAL:PORTmap 1,"A1"
' the main calibration loop ' a description for the connection instructions is read ' and then the standard is acquired dim steps, strPrompt scpi.Parse "sens:corr:coll:guid:init" steps=scpi.Parse ("sens:corr:coll:guid:steps?") wscript.echo "Number of Steps = " + cstr(steps) if (steps > 0) then ' otherwise an error condition occurred for i = 1 to steps strPrompt = scpi.Parse ("sens:corr:coll:guid:desc? " + CStr(i)) MsgBox strPrompt, vbOKOnly, step scpi.Parse ("sens:corr:coll:guid:acq STAN" + CStr(i)) next scpi.Parse "sens:corr:coll:guid:save" MsgBox ("Cal is done!") end if
|
Last Modified:
|
19-Feb-2013 |
Remove Mixer Char only |
|
1-Dec-2011 |
Added commands to choose cal kit for char mixer |
|
12-Sep-2011 |
Fix port 2 Mech Cal kit |
|
5-Apr-2011 |
Edited for ECal |
|
16-Feb-2011 |
Modifications for A.09.33 |