This example performs a VMC Mixer Characterization ONLY.
To run this example program without error:
Replace the ECal module model and serial number with that of your own, or a mechanical cal kit model.
Store a 'default.csa' instrument state file on the PNA with the setup information for your mixer. Or add mixer setup information to this program. See an example.
The SCPI commands in this example are sent over a COM interface using the SCPIStringParser object. You do NOT need a GPIB connection to run this example.
This VBScript (*.vbs) program can be run as a macro in the PNA. To do this, copy the following code into a text editor file, such as Notepad, and save it on the PNA hard drive as *.vbs.
Learn how to setup and run the macro.
See Other SCPI Example Programs
|
Dim app Dim scpi ' Create / Get the PNA application. Set app = CreateObject("AgilentPNA835x.Application") Set scpi = app.ScpiStringParser scpi.Parse "MMEM:LOAD 'default.csa'"
' Perform Cal
' Define the connector and calkit for port 1 of the VNA scpi.Parse "sens:corr:coll:guid:conn:port1 'APC 3.5 female'" scpi.Parse "sens:corr:coll:guid:ckit:port1 'N4691-60004 ECal 02593'" ' Define the connector and calkit for the mixer output port scpi.Parse "sens:corr:coll:guid:conn:port3 'APC 3.5 female'" scpi.Parse "sens:corr:coll:guid:ckit:port3 'N4691-60004 ECal 02593'" ' Select a characterization only calibration. This produces an s2p ' file of the mixer - so the mixer can be used as a calibration ' mixer for the VMC calibration ' The outcome of the calibration is an S2P file. scpi.Parse "SENS:CORR:COLL:GUID:VMC:OPER 'CHAR'" scpi.Parse "SENS:CORR:COLL:GUID:VMC:MIXer:CHAR:CAL:FIL 'C:/Program Files/Keysight/Network Analyzer/Documents/MyMixer.s2p'" ' Set ECal Auto orientation ON scpi.Parse "SENS:CORR:PREF:ECAL:ORI ON" ' For the mixer char step ONLY, ' Auto orientation is turned OFF by the PNA. ' Otherwise it would fail because of the loss of the mixer. ' Manually set the ECal orientation for that step. scpi.Parse "SENS:CORR:COLL:GUID:VMC:MIXer:ECAL:PORTmap 1,'B1'" ' the main calibration loop ' a description for the connection instructions is read ' and then the standard is acquired dim steps, strPrompt scpi.Parse "sens:corr:coll:guid:init" steps=scpi.Parse ("sens:corr:coll:guid:steps?") wscript.echo "Number of Steps = " + cstr(steps) if (steps > 0) then ' otherwise an error condition occurred for i = 1 to steps strPrompt = scpi.Parse ("sens:corr:coll:guid:desc? " + CStr(i)) MsgBox strPrompt, vbOKOnly, step scpi.Parse ("sens:corr:coll:guid:acq STAN" + CStr(i)) next scpi.Parse "sens:corr:coll:guid:save" MsgBox ("Cal is done!") end if |
Last Modified:
|
9-Aug-2013 |
Added ECal orientation command and comments |
|
19-Feb-2013 |
New topic |