This program does the following:
Setup a Noise Figure SC21 Measurement
Calibrate Noise Figure channel
Optional - Configure for an Embedded LO
To run this program, make the following edits, highlighted in yellow:
Set hostname to your PNA computer name
Set tunerECal and pullECal to your ECal model and info
Set ENR to correct file name and location
Set connector types for ECal, power sensor, and noise source
This program can be run as a macro in the PNA. To do this, copy the code into a text editor file such as Notepad and save on the PNA hard drive as NFX.vbs. Learn how to setup and run the macro.
See Other SCPI Example Programs
|
option explicit dim app dim hostname dim parser hostname = "MyPNA" set app = CreateObject("Agilentpna835x.application", hostname) set parser = app.ScpiStringParser ' ecal and noise tunner dim tunerEcal dim sParamECal tunerECal = "N4691-60003 ECal 00591" sParamECal = "N4693-60001 User 2 ECal 00012" ' ENR file dim ENRFile ENRFile = "C:/Program Files/Keysight/Network Analyzer/Noise/346C_44420601.enr" call SetupNFX 'optional if not doing embedded LO 'call SetupEmbeddedLO call CalNFX
sub SetupNFX 'Create NF and SC21 traces parser.Parse "*RST" parser.Parse "CALC:PAR:DEL:ALL" parser.Parse "CALC:CUST:DEF 'NF', 'Noise Figure Converters', 'NF' " parser.Parse "DISP:WIND:TRAC1:FEED 'NF'" parser.Parse "CALC:CUST:DEF 'SC21', 'Noise Figure Converters', 'SC21' " parser.Parse "DISP:WIND:TRAC2:FEED 'SC21' " parser.Parse "SENS:SWE:MODE SING"
'set channel properties ' set sweep type to linear sweep parser.Parse "SENS:SWE:TYPE LIN" ' set number of points parser.Parse "SENS:SWE:POIN 101" ' set IFbandwidth parser.Parse "SENS:BWID 1e3"
'set nfx properties ' turn averaging on parser.Parse "SENS:NOIS:AVER:STAT ON" ' noise averaging factor parser.Parse "SENS:NOIS:AVER 40" ' noise tuner ecal module parser.Parse "SENS:NOIS:TUN:ID '" & tunerECal & "' " ' noise tuner input parser.Parse "SENS:NOIS:TUN:INP 'B' " ' noise tuner output parser.Parse "SENS:NOIS:TUN:OUTP 'A' " ' noise bandwidth parser.Parse "SENS:NOIS:BWID 8e6" ' low gain of noise receiver parser.Parse "SENS:NOIS:GAIN 0" ' sweep single parser.Parse "SENS:SWE:MODE SING"
' Mixer settings parser.Parse "SENS:MIX:INPut:FREQ:MODE SWEPt" parser.Parse "SENS:MIX:INPut:FREQ:STAR 3.6e9" parser.Parse "SENS:MIX:INPut:FREQ:STOP 3.9e9" parser.Parse "SENS:MIX:LO:FREQ:MODE FIXED" parser.Parse "SENS:MIX:LO:FREQ:FIX 1e9" parser.Parse "SENS:MIX:LO:POW 10" parser.Parse "SENS:MIX:OUTP:FREQ:SID LOW" parser.Parse "SENS:MIX:CALC Output" parser.Parse "SENS:MIX:APPLY" 'First apply the settings, then set LO Name parser.Parse "SENS:MIX:LO:NAME 'Port 3'" parser.Parse "SENS:MIX:APPLY" parser.Parse "SENS:MIX:SAVE "C:/Program Files/Keysight/Network Analyzer/Documents/Mixer/MyMixer.mxrx"" ' sweep single parser.Parse "SENS:SWE:MODE SING" end sub
sub CalNFX ' dut connector parser.Parse "SENS:CORR:COLL:GUID:CONN:PORT1 'APC 3.5 female'" parser.Parse "SENS:CORR:COLL:GUID:CONN:PORT2 'APC 3.5 female'" ' port calkits parser.Parse "SENS:CORR:COLL:GUID:CKIT:PORT1 '" & sParamECal & "' " parser.Parse "SENS:CORR:COLL:GUID:CKIT:PORT2 '" & sParamECal & "' "
' power sensor connector parser.Parse "SENS:CORR:COLL:GUID:PSEN1:CONN 'APC 3.5 female'" ' power sensor adapter calkit parser.Parse "SENS:CORR:COLL:GUID:PSEN1:CKIT '" & sParamECal & "' " ' disable LO power cal parser.Parse "SENS:CORR:COLL:NOIS:LO:PCAL 0" ' power calibration power level parser.Parse "SENS:CORR:COLL:GUID:PSEN1:POW:LEV -20"
' noise source connector parser.Parse "SENS:NOIS:SOUR:CONN 'APC 3.5 male'" ' noise source adapter cal calkit parser.Parse "SENS:NOIS:SOUR:CKIT '" & sParamECal & "' " ' cal method parser.Parse "SENS:NOIS:CAL:METH 'Vector'" ' ENR file parser.Parse "SENS:NOIS:ENR:FIL '" & ENRFile & "' "
' set force both adapter cals de-embed to false parser.Parse "SENS:CORR:COLL:NOIS:ENR:ADAP:DEEM 0" parser.Parse "SENS:CORR:COLL:NOIS:PSEN:ADAP:DEEM 0" ' initialize guided cal parser.Parse "SENS:CORR:COLL:GUID:INIT"
' step through calsteps dim steps steps = parser.Parse("SENS:CORR:COLL:GUID:STEP?") dim i, str for i = 1 to steps str = parser.Parse("SENS:CORR:COLL:GUID:DESC? " & i) msgbox str parser.Parse "SENS:CORR:COLL:GUID:ACQ STAN" & i next
parser.Parse "SENS:CORR:COLL:GUID:SAVE 0" parser.Parse "SENS:SWE:MODE CONT" end sub
sub SetupEmbeddedLO ' embedded LO properties ' normalize point parser.Parse "SENS:MIX:ELO:NORM:POIN 101" ' set tuning mode to broadband and precise parser.Parse "SENS:MIX:ELO:TUN:MODE BRO" ' tuning ifbw parser.Parse "SENS:MIX:ELO:TUN:IFBW 3e4" ' max tuning iterations parser.Parse "SENS:MIX:ELO:TUN:ITER 5" ' tuning tolerance parser.Parse "SENS:MIX:ELO:TUN:TOL 1" ' tuning interval parser.Parse "SENS:MIX:ELO:TUN:INT 1" ' turn on ELO parser.Parse "SENS:MIX:ELO:STAT 1" ' sweep single parser.Parse "SENS:SWE:MODE SING" end sub
|