This example sets the sliding load behavior, then performs a Guided Calibration that uses a sliding load.
A measurement must first be set up with desired frequency range, power, and so forth, ready to be calibrated.
The SCPI commands in this example are sent over a COM interface using the SCPIStringParser object. You do not need to control the PNA via GPIB to run this example.
This VBScript (*.vbs) program can be run as a macro in the PNA. To do this, copy the following code into a text editor file, such as Notepad, and save it on the PNA hard drive as guided.vbs.
Learn how to setup and run the macro.
|
Set app = CreateObject("AgilentPNA835x.Application") Set scpi = app.ScpiStringParser ' Specify that any sliding loads should be measured using the ' remote iterative method rather than launching sliding load dialog. scpi.Execute "sens:corr:coll:guid:pref:slid iter" scpi.Execute "sens:corr:coll:guid:conn:port1 ""APC 3.5 female"" " scpi.Execute "sens:corr:coll:guid:conn:port2 ""APC 3.5 male"" " ‘ 85052B cal kit uses sliding loads scpi.Execute "sens:corr:coll:guid:ckit:port1 ""85052B"" " scpi.Execute "sens:corr:coll:guid:ckit:port2 ""85052B"" " scpi.Execute "sens:corr:coll:guid:init" numSteps = scpi.Execute("sens:corr:coll:guid:steps?") ' Measure the standards For i = 1 To numSteps step = "Step " + CStr(i) + " of " + CStr(numSteps) strPrompt = scpi.Execute("sens:corr:coll:guid:desc? " + CStr(i)) MsgBox strPrompt, vbOKOnly, step minIterations = scpi.Execute("sens:corr:coll:guid:iter:min? " + CStr(i)) For j = 1 To minIterations If minIterations > 1 Then MsgBox “Adjust/position the standard for measurement “ + CStr(j) + “ of “ + CStr(minIterations), vbOKOnly scpi.Execute "sens:corr:coll:guid:acq STAN" + CStr(i) Next iterationCount = scpi.Execute("sens:corr:coll:guid:iter:coun? " + CStr(i)) If iterationCount <> minIterations Then MsgBox “Unexpected error!”, vbOKOnly, step scpi.Execute "sens:corr:coll:guid:iter:res " + CStr(i) End If Next ' Conclude the calibration scpi.Execute "sens:corr:coll:guid:save" |
Last modified:
|
4-Dec-2012 |
New topic |