This example sets Phase Reference Cal properties, then performs a Phase Reference calibration.
It is NOT necessary to create an SMC measurement before performing a remote Phase Reference Cal. It is necessary when performed from the user interface.
The SCPI commands in this example are sent over a COM interface using the SCPIStringParser object. You do NOT need a GPIB connection to run this example.
This VBScript (*.vbs) program can be run as a macro in the PNA. To do this, copy the following code into a text editor file, such as Notepad, and save it on the PNA hard drive as *.vbs.
Learn how to setup and run the macro.
See Phase Reference Cal SCPI commands
Learn about SMC with Phase Ref Cal
See Other SCPI Example Programs
|
Set app = CreateObject("agilentpna835x.application") SET s = app.scpistringparser s.parse "SYST:PRES" s.parse "SENS:SWE:MODE HOLD" 'Set cal params s.parse "SYST:CAL:PHAS:RESet" s.parse "SYST:CAL:PHAS:FREQ:STAR 1e9" s.parse "SYST:CAL:PHAS:FREQ:STOP 10E9" ' Read then set the phase ref ID ' Change this to your phase ref name s.parse "SYST:CAL:PHAS:REF 'MYPILOT44'" s.parse "SYST:CAL:PHAS:POW:ATT 10" s.parse "SYST:CAL:PHAS:CONN 'APC 3.5 female'" s.Parse "SYST:CAL:PHAS:CKIT '85052D'" ' turn on port 4 as well. Port 1 and Port 2 are always on s.parse "SYST:CAL:PHAS:PORT4 on" ' Uncomment the following line to use ' an unknown mixer to measure below 55 Mhz. ' If the unknown mixer cal is ON, then the start frequency of the ' entire calibration is always 10 Mhz ' s.parse "SYST:CAL:PHAS:UNKN:INCLude ON" ' Read chan num then begin guided cal chan = s.parse("SYST:CAL:PHAS:GUID:CHAN?") header = "SENS" & CInt(chan) & ":CORR:COLL:GUID:" S.parse header & "INIT" steps = s.parse(header & "STEPS?") wscript.echo steps ' Acquire stds for i = 1 to steps Msgbox s.parse(header & "DESC? " & i) s.parse header & "ACQ STAN" & i next s.parse header & "SAVE:CSET 'scpi_phase_reference'" msgbox "done"
|
Last modified:
|
24-Apr-2013 |
Updated for A.09.90 |
|
1024-Apr-2013 |
New topic |