Save /Recall | Manage Files | Manage Folders | Print | Read Clock
Preset (User) | Security | Configure
Conf Ext Devices: | Sources | PMAR | DC Devices | PulseGens
Hdwr & Capabilities | Macros | Status | Events | Rear Panel | Read Temperature | GPIB Pass-through | VISA Pass-through | Preferences
LXI | Error Messages | mmWave
|
SCPI |
COM |
|
|---|---|---|
|
Preset |
||
|
Preset plus delete window |
||
|
User Preset |
||
|
Load User Preset file |
||
|
Save Current state as User Preset |
||
|
Enable Front Panel for User Preset |
||
|
Quit application |
|
|
Frequency Blanking |
||
|
Local Lockout |
||
|
Set and return GPIB address |
None |
|
|
Set PNA to GPIB system controller or talker/listener |
None |
|
|
Set and return SICL address |
None |
|
|
Control the PNA via SICL |
None |
|
|
Return Full computer name |
None |
|
|
System Impedance |
||
|
Load Test Set Config file and Restart PNA. |
||
|
Hardware |
||
|
IO Configuration |
None |
|
|
Adds an external device to the system. |
||
|
Returns names of all configured devices |
||
|
Set driver for the external device. |
||
|
Set type of device. |
||
|
Configuration path for external device. |
||
|
Enable or disable communication with device. |
||
|
Activation state of the device. |
||
|
Time out value for external device. |
||
|
Remove a device |
||
|
Save configuration file |
||
|
Load configuration file |
||
|
Returns if specified device responds |
||
|
Set Dwell per Point |
||
|
Set Trigger Mode |
||
|
Set Trigger Port |
||
|
Power Meter As Receiver (PMAR) Config See commands to configure and specify a Non- PMAR Power Sensor |
||
|
Enable use of internal cal factors |
||
|
Enable min and max freqs |
||
|
Set Max freq |
||
|
Set Min freq |
||
|
Set max number of PM readings |
||
|
Set tolerance level |
||
|
Select sensor |
||
|
Set Cal Factor data |
||
|
Set Cal Factor frequencies |
||
|
Set Power loss data |
||
|
Set Power loss frequencies |
||
|
Enable Power loss data |
||
|
Set reference cal factor |
||
|
Set Zero method |
None |
|
|
Perform Cal |
None |
|
|
|
|
|
|---|---|---|
|
Sets and returns the current limit value |
||
|
Sets and returns the voltage limit value |
||
|
Correction ON/OFF |
||
|
Offset correction value. |
||
|
Scale correction value. |
||
|
DC Type (Units). |
||
|
Dwell Before/After Point |
||
|
Dwell Before Sweep value |
||
|
Set and return the DC Meter/DC Source Abort Sweep command |
||
|
Set and return the DC Meter/DC Source After Sweep command |
||
|
Set and return the DC Meter/DC Source Before Sweep command |
||
|
Set and return the DC Meter/DC Source Error Query command |
||
|
Set and return the DC Meter/DC Source Disable I/O command |
||
|
Set and return the DC Meter/DC Source ID Query command |
||
|
Set and return the DC Meter/DC Source Enable I/O command |
||
|
Set and return the DC Source maximum output |
||
|
Set and return the DC Source maximum output state |
||
|
Set and return the DC Source minimum output |
||
|
Set and return the DC Source minimum output state |
||
|
Set and return the Point Read commands and Point Set commands |
|
|
|
|
|---|---|---|
|
PG Names catalog |
||
|
Read the integer of the name |
Not applicable |
|
|
Set output channel |
||
|
Set output Hi amplitude (volts) |
||
|
Set output Low amplitude (volts) |
||
|
Set load impedance |
||
|
Set source impedance |
||
|
Master Mode |
||
|
Optional Name/ID argument added to some Pulse gen commands. |
|
DSP Revision |
||
|
DSP FPGA |
||
|
CPU Speed |
||
|
Hostname |
||
|
Many queries regarding the capability of a specific VNA |
||
|
Execute Macro |
||
|
Delete Macro |
||
|
Write macro path, argument, and title |
||
|
Read macro path, argument, and title |
||
|
Status Registers |
N/A |
|
|
*OPC;*WAI |
N/A |
|
|
AllowAllEvents Method |
|
|
|
AllowEventCategory Method |
|
|
|
AllowEventMessage Method |
|
|
|
AllowEventSeverity Method |
|
|
|
DisallowAllEvents Method |
|
|
|
MessageText Method |
|
|
|
OnCalEvent |
|
|
|
OnChannelEvent |
|
|
|
OnDisplayEvent |
|
|
|
OnHardwareEvent |
|
|
|
OnMeasurementEvent |
|
|
|
OnSCPIEvent |
|
|
|
OnSystemEvent |
|
|
|
OnUserEvent |
|
|
|
SetFailOnOverRange |
|
|
|
Material Handler I/O Connector |
||
|
External Test Set Connector |
||
|
Power I/O Connector - Analog IN/Out |
||
|
Read temperature on the receiver microcircuit. |
||
|
Open a GPIB pass-through session |
|
|
|
Write string data to the GPIB pass-through device. |
|
|
|
Write data to the GPIB pass-through device - with header. |
|
|
|
Write data to the GPIB pass-through device - without header. |
|
|
|
Reads string data from the GPIB pass-through device. |
|
|
|
Closes a GPIB pass-through session |
|
|
|
Closes ALL GPIB pass-through sessions |
|
|
|
Open a VISA pass-through session |
||
|
Write string data to the VISA pass-through device. |
||
|
Write data to the VISA pass-through device - without header. |
||
|
Returns list of visa address strings or aliases. |
||
|
Sets timeout value for VISA pass-through commands. |
||
|
Reads string data from the VISA pass-through device. |
||
|
Reads data from the VISA pass-through device as a Safe Array of variants. |
None |
|
|
Reads binary data in a more compact form of Safe Array. |
None |
|
|
Closes a VISA pass-through session |
||
|
Closes ALL VISA pass-through sessions |
||
|
Reset Preference default settings |
None |
|
|
Selected trace is wider. |
None |
None |
|
Selected trace changes width briefly. |
None |
None |
|
Cal: Auto-save User Cal Set |
||
|
Cal: For Guided Cal, set external trigger. |
||
|
Cal: For Unguided Cal, set external trigger. |
||
|
Cal: Simulated Cal Behavior |
None |
|
|
Cal: Use Primary FOM (for mmWave) |
||
|
Memory: Sets and reads the state of the memory data interpolation default preference |
||
|
Memory: Data Math 8510 Mode |
None |
None |
|
Meas: Mathematical offset for receiver attenuation |
||
|
Meas: Mathematical offset for source attenuation |
||
|
Meas: RF power On during frequency sweep retrace |
||
|
Meas: Power Sweep Retrace |
||
|
Meas: External Trigger OUT is Global |
||
|
Meas: Port 1 Noise Tuner Switch state |
||
|
Meas: Draw failed trace segments in red |
||
|
Meas: Draw limit lines in red |
||
|
Marker: Programming treats Mkr 10 as Reference |
||
|
Markers: On Preset, Coupled Markers is ON |
||
|
Markers: On Preset, Coupling Method is Channel |
||
|
Markers: Coupling controls on|off state of markers. |
||
|
Report source unleveled events as errors |
||
|
Ext Device: de-activate on PRESET and recall. |
||
|
On PRESET set two-point group delay aperture |
||
|
On PRESET always turn power ON |
||
|
On PRESET show Quick Start dialog |
||
|
Report when receiver is overloaded |
||
|
Turn source power OFF when receiver is overloaded |
||
|
More buttons |
||
|
Define Data Saves |
||
|
User Preset |
||
|
User Key |
None |
None |
|
Printer Page Setup |
None |
|
|
Millimeter settings |
None |
None |
|
Power Limit |
||
|
Display and Print Colors |
||
|
Returns Structured status of the PNA networking configuration. |
None |
|
|
Returns string status of the PNA networking configuration. |
None |
|
|
Resets the PNA LAN configuration. |
None |
|
|
Modifies settings of the PNA computer networking configuration. |
None |
|
|
Displays the LAN Status dialog with LAN Status Indicator showing IDENTIFY. |
||
|
Enable the display of Error Messages |
None |
|
|
Timed vs Dialog messages |
None |
None |
Millimeter-Wave Commands |
||
|
|
None |
|
|
None |
||
|
None |
||
|
None |
||
|
None |
||
|
None |
||
|
None |
||
|
None |
||
|
None |
||
|
None |
||
|
None |
||
|
None |
||
|
None |
||
|
None |
||
|
None |
||
|
None |
||
|
None |
||
|
None |
||
|
None |
||
|
None |
||
|
None |
||
|
None |
||