Only the Main and Leveling & Offsets Power commands corresponding to the Swept IMD and Swept IMD Converters measurement classes are documented here. The Port Power and Attenuators commands are identical to the Port Power and Attenuator commands for the Standard measurement class and can be accessed by clicking on the softtab on the graphic below.
Click here to view links to Power commands for all Measurement Classes.
| Main Tab Commands | |||
| Softkey | Sub-item | SCPI | COM |
| Tone Power | SENSe:IMD:TPOWer:F1 SENSe:IMD:TPOWer:F2 | ||
| RF Power | ON/OFF | OUTPut[:STATe] | |
| Start Power | SOURce:POWer:PORT:STARt | ||
| Stop Power | SOURce:POWer:PORT:STOP | ||
|
|||
| IMD Setup... (Swept IMD Measurement Class only) |
|
||
| IMDX Setup... (Swept IMD Converters Measurement Class only) |
|
||
| Leveling & Offsets Tab Commands | |||
| Softkey | Sub-item | SCPI | COM |
| Select | Port 1 | None |
None |
| Port 2 | None |
None |
|
| Port 3 | None |
None |
|
| Port 4 | None |
None |
|
| Port 1 Src2 | None |
None |
|
| Source3 | None |
None |
|
| Offset | SOURce:POWer:ALC[:MODE]:RECeiver:OFFSet | ||
| Limit | ON/OFF | SYSTem:POWer:LIMit:STATe | |
| Power Limit | SYSTem:POWer:LIMit | ||
|
|||
| ALC Hardware | Internal | SOURce:POWer:ALC[:MODE] | |
| Open Loop | SOURce:POWer:ALC[:MODE] | ||
|
|||