Write/Read
About Power Sweep

StartPower Property


Description

Sets the start power of the analyzer when sweep type is set to Power Sweep. Frequency of the measurement is set with chan.CWFrequency.

 VB Syntax

object.StartPower = value

Variable

(Type) - Description

object

One of the following:

value

(double) - Start Power in dBm.

Note: The range of settable power values depends on the VNA model and if source attenuators are installed. To determine the range of values, use cap.MaximumSourceALCPower and cap.MinimumSourceALCPower

Auto attenuation is not allowed in Power Sweep.

Return Type

Double

Default

0

Examples

Chan.StartPower = -10 'Write

strtpwr = Chan.StartPower 'Read

C++ Syntax

HRESULT get_StartPower(double *pVal)
HRESULT put_StartPower(double newVal)

Interface

IChannel

|CalSet3